AXIS#.TEMP

Description

This parameter returns the measured temperature of the power module on the power board for the associated axis.

Examples

Usage

The parameter can be used to track board temperatures as they change during drive operation. There is at least one control board temperature measurement (e.g., DRV.TEMP) and one power board temperature measurement (e.g., AXIS1.TEMP).

Code

--> DRV.TEMP
52.367 (Control) [degC]
--> AXIS1.TEMP
31.664 (Power1) [degC]
--> AXIS2.TEMP
32.312 (Power2) [degC]

Versions

Action Version Notes
Implemented 02-02-02-000

 

General Information

Type

Read Only

Units

degC

Range

N/A

Default Value

N/A

Data Type

Float

Stored in Non-Volatile Memory

No

Variants Supported

All variants are supported.

Industrial Ethernet Information

EtherCAT CoE and CANopen

Command

Index

SubIndex

Data Type

Units

Float Scale

Access

PDO Mappable

AXIS1.TEMP

5000h

10h

Signed32

-

-

Read only

No

AXIS2.TEMP

5100h

10h

Signed32

-

-

Read only

No

EtherNet/IP

ID

Instance

Attribute

Name

Data Type

Access

User Mappable

5026

1

5026 (0x13a2)

AXIS1.TEMP

Signed32

Read Only

Yes

70562

2

5026 (0x13a2)

AXIS2.TEMP

Signed32

Read Only

Yes

PROFINET

Parameter

PNU

Data Type

Access

Units

AXIS#.TEMP

5026

Float

Read Only

-